Hello,
My customer would like to put a 4MByte ASRAM on the EMIF1.
It would be glad if 2MWord*16bit (A[20:0], DQ[15:0]) type is good. They have many parts in their inventory.
Then we are looking into the DS, Table 6-3 EMIF Chip Select Memory Map.
We find a sentence, "If 16-bit memory is used, then the maximum size is 1M x 16."
The sentence would say the EMIF doesn’t accept ASRAMs of 2MWord*16bit.
On the other hand the DS p.23, we find EM1A19. From the terminal I would expect
the address signals could be connected as follows:
(F28075 EMIF1) - - - (ASRAM)
EM1A19 - - - A20
EM1A18 - - - A19
. . .
EM1A0 - - - A1
EM1BA[1] - - - A0
- - -
I’m sorry for a long explanation, can I ask two questions?
Q1. Is it possible to connect 2MWord*16bit (A[20:0], DQ[15:0]) type ASRAM to the EMIF1 ?
Q2. Could you please advise how to put a, SRAM of total 4MBytes?
An idea would be to put a couple of half size SRAM, like 1MWord*16bit (A[20:0], DQ[15:0]),
But a better idea would be highly appreciated.