Other Parts Discussed in Thread: CONTROLSUITE
Hello,
I am using TMDSDOCK28379D (F28379D Delfino Experimenter Kit with HSEC180 docking station) and trying to drive a motor with my power electronic circuit. I am using two USB cables. One supplies the control cards while the other supplies docking station. I am able to run the MCU with Matlab 2019a or Matlab 2019b. I am using 68,70 and 74 pins of HSEC180 to send encoder signals to the Simulink. Inside the Simulink, I can generate proper gate signals. Finally, I am using GPIO DO blocks to send the signals to the HSEC180 pins. Although I can send signals to the Simulink via HSEC180, I have never received Simulink signals from HSEC180 pins. I have followed pin map in the file named '180_HSEC8_DV_pinout_R1_1' in the following address:
C:\ti\controlSUITE\development_kits\~ExperimentersKits\120or180pin_HSEC_DockingStn-HWdevPkg_v1_1\R4_1
Do you think my HSEC180 docking station has problem? Do I need to make any switch settings on the MCU? Could you please help me about that?
Thank you