Other Parts Discussed in Thread: TIDM-BLPFC, TMS320F28035
This part number is provided at TI with two different topologies. One with the name TMDSHVBLPFCKIT (http://www.ti.com/tool/TMDSHVBLPFCKIT and the other is with the name TIDM-BLPFC (www.ti.com/.../tidu312.pdf). The user guides or the white papers provided with them have two different topologies. i.e. the first one is given with single Buck topology while the second one is given with interleaved Boost topology. If both of them are their uses of the same device then my question is that with which hardware setup this device is initially provided .i.e. Single Buck (www.ti.com/.../TMDSHVBLPFCKIT) or Interleaved Buck-Boost Topology (www.ti.com/.../tidu312.pdf) My second question is that can I change the default hardware setup to Buck-Boost Toplogy and can arrange the control setup accordingly (as I am working on the Buck-Boost Converter)?