This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28035: tms320f28035

Part Number: TMS320F28035


Hi all,

I has become fed of navigating the internet to find information I need for a coming proejct. I need your help TI.

It is too simple question to answer on.

What are the main differences between TMS320F28035PNS and TMS320F28035PNQ?

we are wavering between those two DSP so, ahead of making a decision, we'd like to know that aforementioned.

 Thanks TI.

I am a big fan of you!

best regard

  • Yoonseok,

    The difference is that the 'Q' version is AEC Q100 qualified.  This is an automotive standard.  Unless your application is automotive and requires a Q grade device, use the S version.  Both S and Q have the same -40C to +125C T_ambient temperature rating.  If you don't need +125C, use the F28035PNT, which is the same as the S except rated for -40C to +105C.

    Regards,

    David