Tool/software: Code Composer Studio
Hi Everyone!
Yay! First time posting from my company account :-).
I'm looking at the TIDM-HV-1PH-DCAC, and I'm hoping that someone can answer a few questions, mostly having to do with the Sigma Delta ADCs.
1) It looks like there's an inductor current sensor and voltage sensing that goes directly to the DSP on board ADCs, and the code indicates that either the on board SAR ADCs or the SD ADCs could be used for real time control, but only the SAR ADCs seem to be activated. Is the real-time control of inductor current and output voltage done with the SAR ADCs or SD ADCs or is it selectable or is a combination used?
2) Inductor current is sensed indirectly with the SD ADCs by adding the output current and the capacitor current- is there a reason why the inductor current wasn't sensed directly?
3) It appears that the oversample rate is 32, and that the filter is SINC3. Is this correct? The clock pins are hooked up to GPIO4, which doesn't appear to be an SDFM clock pin. How are the SD ADCs clocked?
I'm excited to be back on E2E!
Best,
Justin