Other Parts Discussed in Thread: MOTORWARE, , BOOSTXL-DRV8305EVM
Hi,
background: over the years I've used LAUNCHXL-F28027 + BOOSTXL-DRV8305EVM with Motorware Instaspin-foc labs (various versions) with number of different motors and they've all exhibited the same issue.
For number of reasons I've not had the impetus to find the root cause but now I need to.
At the moment I'm working with proj_lab03a.
The motor runs just fine but if accelerate/decelare too quickly then I hear that something goes wrong with the
PWM as a new audible hissing sound is produced by the motor windings and the motor speed no
longer reaches the set speed although the motor does keep running and I can still see all the variables etc with the debugger.
Nothing sort of complete software res-start restores normal operation.
I have
gMotorVars.MaxAccel_krpmps = _IQ(4.0)
and when I change
gMotorVars.SpeedRef_krpm = _IQ(1) => _IQ(4)
sometimes (!) the system goes into this limbo mode, depending on the motor mechanical loading.
Looking at the variables I see nothing that would give a clue what is going on.
So I'm looking for ideas and experience from other users of Motorware.
Not sure if this even the right forum as I expect this ia Motorware software related question.
Oh, ah, one more thing: over the years I've had a number of boards where I've seen the issue so not likely a hardware problem.
cheers Kusti