Part Number: C2000WARE
Hello All,
I am little new in programming micro controllers,
and I am trying to make CAN driver work on TMS320F28379D using the sample code.
I am using the control card as by followed link,
http://www.ti.com/tool/TMDSCNCD28379D
It has a docking station as by attachment,0576.EvalBoard.pdf
I have found the pins from the following Schematic pdf,0638.3580.controlCARDDockingStationR4_1-SCH.pdf
Happily I could able to Tx using the example code,
But couldn't receive messages, If I try transmitting using the SW tool(Peak CAN),
The Bus load immediate shoots up and I get a Bus off warning.
I have double checked the pins connections they seem fine is anything that I can try to make to work?
Thank you,
With Regards,
Arvind.