This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377S: power sequence

Part Number: TMS320F28377S

hi expert,

we see from datasheet, which has description below.

”The voltage on VDDIO should be greater than VDD or no less than 0.3 V below VDD at all times. VDDIO,
VDD3VFL, VDDOSC, and VDDA should be powered up together and be kept within 0.3 V of each other during
operation. Before powering the device, no voltage larger than 0.3 V above VDDIO should be applied to any
digital pin, and no voltage larger than 0.3 V above VDDA should be applied to any analog pin. The VREFHI
voltage should not exceed VDDA at any time.“

however,my customer use 2 devices providing 3.3V power supply. Is there any issues here?provide the power train wavaform below.

Yellow for VDDA,

Blue for VDDIO, VDDOSC and VDD3VFL,

Red for VDD.

And the board can work normal, only some boards have abnormal performance.

could you kindly check if the design has some crutial error.

does it a must to provide 3.3V power together by 1 LDO?

BR

Emma