Hello,
I have changed some hardware to allow a higher pfc_bus voltage and Vac input voltage, the values are shown below.
I am not having any luck getting the unit to run.
What should these values be for the resistor changes I have made.
vienna_settings.h
91 #define VIENNA_VAC_MAX_SENSE_VOLTS ((float32_t)500)
92 #define VIENNA_VDCBUS_MAX_SENSE_VOLTS ((float32_t)1010)
93 #define VIENNA_V_MAX_SENSE_VOLTS ((float32_t)606)
140 #define VIENNA_VBUS_REF_SET_VOLTS ((float32_t)800)
*******************************************************************************************************8
Vbus
Rb changed the resistor to 1.62k
Rd changed the resistor to 9.09k
fVac
Rf changed the resistor to 1.62k
Rh changed the resistor to 9.09k
Thanks
Steve