Other Parts Discussed in Thread: DRV8320
Hi,
Will we have the demo code for InstaSPIN, to support dual motors, on F28002xC?
Another request from powertools market, one motor (10PP) needs to work in two conditions:
1) Normal one, low speed high torque, like 3000RPM, FOC, close loop, like InstaSPIN.
2) Special one, higher speed low torque, like 60000RPM, open loop control, trapezoidal, 10% speed accuracy. It's like PWM duty directly comes from BMEF and comparator.
Can we do?
Thanks a lot.
Br, Jordan