Tool/software: Code Composer Studio
Using an XP machine with a Spectrum Digital XDS510LC USB emulator to connect to the chip, but the connection seems very spotty
I can only get it to connect if I bring up the 1.8V core about 1/2 second slower than the main 3.3V rail... but I think that means there is something either wrong in the .gel file or something else for the part I'm using. The datasheet doesn't make any mention about having to power up the rails at different timing. Also, even when I power up the rails differently I can only get the board to connect about 10% of the time.
For the record the micro I am using is a SM320F2808, which there doesn't seem to be much documentation. I'm using the gel file for a f2808 (a TMS320F instead of a SM320F) but I think that should be ok. The .gel file I have is version 3.30.2
I am open to changing anything at this point. I have no idea why sometimes it will connect and other times it won't. If you have any ideas on drivers or config file versions to use I'm open to anything. Also if there is a better version of CCS that's fine too. I just need to get this working.