Hello,
I am using this microcontroller to digital contol a flyback DC-DC converter. To improve efficiency I want to monitor a voltage which can become negative. I use the following circuit to fit the signal inside the maximum ratings of the input pins of the microcontroller:
Unfortunatily I still get a negative voltage spikes for about 20-40 ns (with a Frequency of 150 kHz). The negative voltage spikes range from -0.5 V to -3.5 V.
I want to compare this signal with the internal COMP. Can its input whitstand such short peaks? A fast response time is very important so I want to avoid additional OPAMS.