This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C: CMPxHR register when AUTOCONV=1

Part Number: TMS320F280049C
Other Parts Discussed in Thread: C2000WARE

Hello C2000 Team,

I am having some confusion concerning use of the HRPWM with the AUTOCONV feature.  I am using F28004x, so following TRM SPRUI33C, example on p.1913.

Step 1 makes sense.  I would perform something like this in C:

float duty=0.405;
int period=80;
CMPx = duty*period;  // CMPx=32

Step 2 is where the confusion is.  In particular, there is a note at the bottom of the example that says:

NOTE: If the AUTOCONV bit (HRCNFG.6) is set and the MEP_ScaleFactor is in the HRMSTEP
register, then CMPAHR / CMPBHR register value = frac (PWMDuty*PWMperiod<<8). The
rest of the conversion calculations are performed automatically in hardware, and the correct
MEP-scaled signal edge appears on the ePWM channel output. If AUTOCONV is not set, the
above calculations must be performed by software.

I'm supposed to compute frac(duty*period<<8)?

Specifically, this is frac( (duty*period)<<8) using order of operations.

frac( (80*0.405)<<8) = frac(32.4 << 8) = frac(8243.2) = 0.2.

This doesn't make sense.  Perhaps it is supposed to be frac(PWMduty*PWMperiod) << 8.  That would be

frac(32.4)<< 8  = (0.4)<<8 = 102

Can someone advise, what is the correct value to put in the CMPxHR register when AUTOCONV=1?

Regards,

David

  • I see. Take a look at this example. When I last worked with HRPWM I had the same confiusion. Here is an example that works with FLOATs.

    //
    // Included Files
    //
    #include "driverlib.h"
    #include "device.h"
    #include "SFO_V8.h"
    
    #define EPWM_TIMER_TBPRD            100UL
    #define MIN_HRPWM_DUTY_PERCENT      4.0/((float32_t)EPWM_TIMER_TBPRD)*100.0
    //
    // Defines
    //
    #define LAST_EPWM_INDEX_FOR_EXAMPLE    5
    
    //
    // Globals
    //
    
    float32_t dutyFine = MIN_HRPWM_DUTY_PERCENT;
    uint16_t status;
    
    int MEP_ScaleFactor; // Global variable used by the SFO library
                         // Result can be used for all HRPWM channels
                         // This variable is also copied to HRMSTEP
                         // register by SFO() function.
    
    volatile uint32_t ePWM[(PWM_CH + 1)] =
        {0, EPWM1_BASE, EPWM2_BASE, EPWM3_BASE, EPWM4_BASE};
    //
    // Function Prototypes
    //
    void initHRPWM(uint32_t period);
    void initEPWMGpio(void);
    void error(void);
    //__interrupt void epwm1ISR(void);
    //__interrupt void epwm2ISR(void);
    //__interrupt void epwm3ISR(void);
    //__interrupt void epwm4ISR(void);
    
    //
    // Main
    //
    void main(void)
    {
        uint16_t i = 0;
    
        //
        // Initialize device clock and peripherals
        //
        Device_init();
    
        //
        // Disable pin locks and enable internal pull ups.
        //
        Device_initGPIO();
    
        //
        // Initialize PIE and clear PIE registers. Disables CPU interrupts.
        //
        Interrupt_initModule();
    
        //
        // Initialize the PIE vector table with pointers to the shell Interrupt
        // Service Routines (ISR).
        //
        Interrupt_initVectorTable();
    
        //
        // Assign the interrupt service routines to ePWM interrupts
        //
        //Interrupt_register(INT_EPWM1, &epwm1ISR);
        //Interrupt_register(INT_EPWM2, &epwm2ISR);
        //Interrupt_register(INT_EPWM3, &epwm3ISR);
        //Interrupt_register(INT_EPWM4, &epwm4ISR);
    
        initEPWMGpio();
    
    
        //
        // CHANGE XBAR inputs from using GPIO0
        // if EPWM SYNCIN is enabled, EXTSYNCIN1 and EXTSYNCIN2 will use
        // GPIO0 (which is the output of EPWM1).
        // Pick and unused GPIO
        //
        XBAR_setInputPin(XBAR_INPUT5, 50);
        XBAR_setInputPin(XBAR_INPUT6, 50);
    
    
        //
        // Calling SFO() updates the HRMSTEP register with calibrated MEP_ScaleFactor.
        // HRMSTEP must be populated with a scale factor value prior to enabling
        // high resolution period control.
        //
        while(status == SFO_INCOMPLETE)
        {
            status = SFO();
            if(status == SFO_ERROR)
            {
                error();   // SFO function returns 2 if an error occurs & # of MEP
            }              // steps/coarse step exceeds maximum of 255.
        }
    
    
    
        //
        // Disable sync(Freeze clock to PWM as well)
        //
        SysCtl_disablePeripheral(SYSCTL_PERIPH_CLK_GTBCLKSYNC);
        SysCtl_disablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC);
    
        initHRPWM(EPWM_TIMER_TBPRD);
    
        //
        // Enable sync and clock to PWM
        //
        SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC);
    
    
        // Enable ePWM interrupts
        //
        //Interrupt_enable(INT_EPWM1);
        //Interrupt_enable(INT_EPWM2);
        //Interrupt_enable(INT_EPWM3);
        //Interrupt_enable(INT_EPWM4);
    
        //
        // Enable Global Interrupt (INTM) and realtime interrupt (DBGM)
        //
        EINT;
        ERTM;
    
    
        for(;;)
        {
             //
             // Sweep DutyFine
             //
             for(dutyFine = MIN_HRPWM_DUTY_PERCENT; dutyFine < 99.9; dutyFine += 0.01)
             {
                 DEVICE_DELAY_US(1000);
                 for(i=1; i<LAST_EPWM_INDEX_FOR_EXAMPLE; i++)
                 {
                     float32_t count = (dutyFine * (float32_t)(EPWM_TIMER_TBPRD << 8))/100;
                     uint32_t compCount = (count);
                     HRPWM_setCounterCompareValue(ePWM[i], HRPWM_COUNTER_COMPARE_A, compCount);
                     HRPWM_setCounterCompareValue(ePWM[i], HRPWM_COUNTER_COMPARE_B, compCount);
                 }
    
                 //
                 // Call the scale factor optimizer lib function SFO()
                 // periodically to track for any change due to temp/voltage.
                 // This function generates MEP_ScaleFactor by running the
                 // MEP calibration module in the HRPWM logic. This scale
                 // factor can be used for all HRPWM channels. The SFO()
                 // function also updates the HRMSTEP register with the
                 // scale factor value.
                 //
                 status = SFO(); // in background, MEP calibration module
                                 // continuously updates MEP_ScaleFactor
    
                 if (status == SFO_ERROR)
                 {
                     error();   // SFO function returns 2 if an error occurs & #
                                // of MEP steps/coarse step
                 }              // exceeds maximum of 255.
             }
         }
    }
    
    //
    // epwm1ISR - ePWM 1 ISR
    //
    //__interrupt void epwm1ISR(void)
    //{
    //    EPWM_clearEventTriggerInterruptFlag(EPWM1_BASE);
    //    Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP3);
    //}
    
    //
    // epwm2ISR - ePWM 2 ISR
    //
    //__interrupt void epwm2ISR(void)
    //{
    //    EPWM_clearEventTriggerInterruptFlag(EPWM2_BASE);
    //    Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP3);
    //}
    
    //
    // epwm3ISR - ePWM 3 ISR
    //
    //__interrupt void epwm3ISR(void)
    //{
    //    EPWM_clearEventTriggerInterruptFlag(EPWM3_BASE);
    //    Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP3);
    //}
    
    //
    // epwm4ISR - ePWM 4 ISR
    //
    //__interrupt void epwm4ISR(void)
    //{
    //    EPWM_clearEventTriggerInterruptFlag(EPWM4_BASE);
    //    Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP3);
    //}
    
    
    
    void initEPWMGpio(void)
    {
        //
        // Configure GPIO0/1 as ePWM1A/1B pins respectively
        //
        GPIO_setPadConfig(0, GPIO_PIN_TYPE_STD);
        GPIO_setPinConfig(GPIO_0_EPWM1A);
        GPIO_setPadConfig(1, GPIO_PIN_TYPE_STD);
        GPIO_setPinConfig(GPIO_1_EPWM1B);
    
        //
        // Configure GPIO2/3 as ePWM2A/2B pins respectively
        //
        GPIO_setPadConfig(2, GPIO_PIN_TYPE_STD);
        GPIO_setPinConfig(GPIO_2_EPWM2A);
        GPIO_setPadConfig(3, GPIO_PIN_TYPE_STD);
        GPIO_setPinConfig(GPIO_3_EPWM2B);
    
        //
        // Configure GPIO4/5 as ePWM3A/3B pins respectively
        //
        GPIO_setPadConfig(4, GPIO_PIN_TYPE_STD);
        GPIO_setPinConfig(GPIO_4_EPWM3A);
        GPIO_setPadConfig(5, GPIO_PIN_TYPE_STD);
        GPIO_setPinConfig(GPIO_5_EPWM3B);
    
        //
        // Configure GPIO6/7 as ePWM4A/4B pins respectively
        //
        GPIO_setPadConfig(6, GPIO_PIN_TYPE_STD);
        GPIO_setPinConfig(GPIO_6_EPWM4A);
        GPIO_setPadConfig(7, GPIO_PIN_TYPE_STD);
        GPIO_setPinConfig(GPIO_7_EPWM4B);
    }
    
    void initHRPWM(uint32_t period)
    {
    
        uint16_t j;
    
        //
        // ePWM channel register configuration with HRPWM
        // ePWMxA / ePWMxB toggle low/high with MEP control on Rising edge
        //
        for (j=1;j<LAST_EPWM_INDEX_FOR_EXAMPLE;j++)
        {
            EPWM_setEmulationMode(ePWM[j], EPWM_EMULATION_FREE_RUN);
    
            //
            // Set-up TBCLK
            //
            EPWM_setTimeBasePeriod(ePWM[j], period-1);
            EPWM_setPhaseShift(ePWM[j], 0U);
            EPWM_setTimeBaseCounter(ePWM[j], 0U);
    
            //
            // set duty 50% initially
            //
            HRPWM_setCounterCompareValue(ePWM[j], HRPWM_COUNTER_COMPARE_A, (period/2 << 8));
            HRPWM_setCounterCompareValue(ePWM[j], HRPWM_COUNTER_COMPARE_B, (period/2 << 8));
    
    
            //
            // Set up counter mode
            //
            EPWM_setTimeBaseCounterMode(ePWM[j], EPWM_COUNTER_MODE_UP);
            EPWM_disablePhaseShiftLoad(ePWM[j]);
            EPWM_setClockPrescaler(ePWM[j],
                                   EPWM_CLOCK_DIVIDER_1,
                                   EPWM_HSCLOCK_DIVIDER_1);
            EPWM_setSyncOutPulseMode(ePWM[j], EPWM_SYNC_OUT_PULSE_DISABLED);
    
    
            //
            // Set up shadowing
            //
            EPWM_setCounterCompareShadowLoadMode(ePWM[j],
                                                 EPWM_COUNTER_COMPARE_A,
                                                 EPWM_COMP_LOAD_ON_CNTR_ZERO);
            EPWM_setCounterCompareShadowLoadMode(ePWM[j],
                                                 EPWM_COUNTER_COMPARE_B,
                                                 EPWM_COMP_LOAD_ON_CNTR_ZERO);
    
            //
            // Set actions
            //
    
            EPWM_setActionQualifierAction(ePWM[j],
                                          EPWM_AQ_OUTPUT_A,
                                          EPWM_AQ_OUTPUT_HIGH,
                                          EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO);
    
    
            EPWM_setActionQualifierAction(ePWM[j],
                                          EPWM_AQ_OUTPUT_B,
                                          EPWM_AQ_OUTPUT_HIGH,
                                          EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO);
    
            EPWM_setActionQualifierAction(ePWM[j],
                                          EPWM_AQ_OUTPUT_A,
                                          EPWM_AQ_OUTPUT_LOW,
                                          EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA);
            EPWM_setActionQualifierAction(ePWM[j],
                                          EPWM_AQ_OUTPUT_B,
                                          EPWM_AQ_OUTPUT_LOW,
                                          EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPB);
    
    
            HRPWM_setMEPEdgeSelect(ePWM[j], HRPWM_CHANNEL_A, HRPWM_MEP_CTRL_FALLING_EDGE);
            HRPWM_setMEPControlMode(ePWM[j], HRPWM_CHANNEL_A, HRPWM_MEP_DUTY_PERIOD_CTRL);
            HRPWM_setCounterCompareShadowLoadEvent(ePWM[j], HRPWM_CHANNEL_A, HRPWM_LOAD_ON_CNTR_ZERO);
    
            HRPWM_setMEPEdgeSelect(ePWM[j], HRPWM_CHANNEL_B, HRPWM_MEP_CTRL_FALLING_EDGE);
            HRPWM_setMEPControlMode(ePWM[j], HRPWM_CHANNEL_B, HRPWM_MEP_DUTY_PERIOD_CTRL);
            HRPWM_setCounterCompareShadowLoadEvent(ePWM[j], HRPWM_CHANNEL_B, HRPWM_LOAD_ON_CNTR_ZERO);
    
            HRPWM_enableAutoConversion(ePWM[j]);
    
            //
            // Turn off high-resolution period control.
            //
    
            HRPWM_disablePeriodControl(ePWM[j]);
            HRPWM_disablePhaseShiftLoad(ePWM[j]);
    
    
            //
            // Interrupt where we will change the Compare Values
            // Select INT on Time base counter zero event,
            // Enable INT, generate INT on 1st event
            //
            //EPWM_setInterruptSource(ePWM[j], EPWM_INT_TBCTR_ZERO);
            //EPWM_enableInterrupt(ePWM[j]);
            //EPWM_setInterruptEventCount(ePWM[j], 1U);
        }
    
    }
    
    //
    // error - Halt debugger when called
    //
    void error (void)
    {
        ESTOP0;         // Stop here and handle error
    }
    
    

  • Hi Nima,

    Thank you for the example.  This helps.  It looks like one of the examples from C2000Ware, but using float instead of fractions.

    Do you happen to have the complete project in a portable format that you could send? (i.e., the .c file and the project spec)

    Regards,

    David

  • David,

    For the CCS project, you can import an existing epwm project from the driverlib examples.

    Add the SFO_v8_fpu_lib_build_c28_driverlib_eabi.lib from C2K/libraries/calibration

    Add the C2K/libraries/calibration.../include to the directory paths.

    Here is an attached example project but it will have some paths that will need updating.

    hrpwm.zip