Part Number: TMS320F280025C
Hi,
I have a few questions from my customer who is designing their own board now.
Q1) VDD decoupling capacitors:
According to datasheet,
“TI recommends placing a decoupling capacitor near each VDD pin with a total capacitance of approximately 22 μF.”
Customer wants to make sure each VDD pin needs to be connected together or not.
If not, how the 22uF should be distributed for each VDD pin?
ex. Suppose 48 QFP, there are two VDD pins. 2uF for one pin and 20uF for another pin is acceptable?
Q2) Unused AIO pins:
It is not clear how to handle unused AIO pins. They are not listed in datasheet Table 4-9.
Is this OK to connect VSS?
Q3) VREFHI pin usage:
In case internal reference is used, adding 2.2uF capacitor is enough, right?
Thanks and regards,
Koichiro Tashiro