Tool/software: Code Composer Studio
hello ,
I meet some problems when I run parameter identification for a pmsm using TI FAST on tms320f28054f .
I have konwn the motor's Rated current is 16A,I defined the est data in user.h as below:
USER_MOTOR_RES_EST_CURRENT (3.4) //(10%*16*1.414)
but I find the current output on the oscilloscope can only reach about 2A when it is in the state of EST_State_Rs .however the there is no problem in the state of EST_State_RoverL and the current output can reach 1.7A (as described in the datasheet : 50% of the USER_MOTOR_RES_EST_CURRENT ).
Now I can't find Which parameter limits the current output on the state of EST_State_Rs,Any insights would be greatly appreciated.