Hi,
Please let me know which programmer can I use for programming
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Vinoth,
There are primarily two ways to program the flash (3, if you include SPI method, but it is a bit more involved), JTAG & Serial port.
If you have a working copy of CCSv3.3, you could program via the Flash plugin (i.e. the tool built into CCS itself)
Helpful information is available at:
https://www.ti.com/tool/FTLF240X
https://www.ti.com/tool/SPRC074
If programming via JTAG is not an option, Serial Programming solutions are available from 3rd parties:
Hi Hareesh,
Thanks for your reply. which hardware can I use C2 prog for Ic programming.
Easiest (and free) option is to use the SCI port. Please refer to the FAQ section for details. https://www.codeskin.com/c2prog-faq