This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28027F: f28027

Part Number: LAUNCHXL-F28027F

Hi,

I have accidently connected 5V pin to ADC pin of launchpad. After that launchpad turns on for little time(4,5 seconds) the it turns off automatically. The voltages starts to drop constantly on both 5V pin and 3.3v pin. What's the solution?

  • Ahsan,

    you have likely caused an EOS event inside of the device. If true the device is permanently damaged.

    You can try re-soldering a new C2000 device onto the LaunchPad, but this is not recommended unless you have previous experience.


    I would recommend getting a new LaunchPad.

    Regards,
    Cody