This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMDSCNCD280025C: onboard debugger does not connet to the TMS320F280025C

Part Number: TMDSCNCD280025C
Other Parts Discussed in Thread: TMS320F280025C

Tool/software: Code Composer Studio

We got a fresh

TMS320F280025C controlCARD evaluation module and a

HSEC180 controlCARD Baseboard Docking Station

We put the board in the card and connect the board USB to power the system.

We connect controlCARD USB to use the onboard XDS100v2.

S1A is on -  for the debugger. The LEDs D2A and D3 are on.

The blue LEDs D3A and D4A light a little bit.

The Win10 PC found the onboard XDS100v2 interface.

But the communication between the XDS100v2 and the CPU seems not working. The communication check fails.

Is there anything additional to set, that the CPU start working?

I'm concerned that there is a power problem, because Win10 had reported, that too much current was required.
I read it in the ocumentation. But I'm the meaning, that it is only a problem with additional peripherials. Without them I was the meaning
that the power consumtion is below 500mA.