Part Number: TMS320F28069
dear expert,
there is a question about ADC sample rate of 28069 and 280049. As show in datasheet, sample rate of 28069 is 3.46M, and 280049 is 3.45M.
For 28069, ADC converion time is 13 ADCCLKs(45MHz), then sample rate = 1/(13/45M)=3.46M.
For 280049, ADC conversion time is 21 SYSCLKs (100MHz), and S/H time is 8 SYSCLKs, then the sample rate = 1/[(21+8)/100M]=3.45M.
So which one is correct, if 280049 is correct, then the sample rate of 28069 is below 3.46M, because the ADC sample time is 7 ADCCLKs at least.