Other Parts Discussed in Thread: TMS320F28335, TIDM-02006
Dear Sir,
we have deployed by now a large number of ECS solutions based on the combination of the MCU (TMS320F28335) and PLD (Artix 7 series) devices, closely interconnected by synchronously operated communication bus, and by a quite a few discrete signal lines (to enhance flexibility and configurability of the ECS core module, as well as to extend the CPU capabilities of the MCU...). Since there are still some spare IO pins within the target system interface (considered so far as a special reserve), I kindly ask you to provide me information on the possibility to upgrade the previously described ECS core module by FSI compliant interface (operating at frequencies up to 50 MHz). Is it possible to implement more than one such FSI compliant interface (like few transmit and receive ports provided by F28388D MCUs)?
Best regards
Nenad