This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

2MTR-DYNO: Current rating of power supply

Part Number: 2MTR-DYNO
Other Parts Discussed in Thread: BOOSTXL-DRV8305EVM,

Hi Team,

A customer has 2MTR-DYNO evaluation kit. The M-2310P-LN-04K motor included in the kit is rated at 60V, 7.1A. However, the BOOSTXL-DRV8305EVM driving the motor is rated at 45V, 15A RMS (20A peak) drive current. The customer would like to request for the specifications of the power supply to power this kit. He plans to power the two motors simultaneously.

Regards,

Danilo