Other Parts Discussed in Thread: AMC1210
Hi Team C2000,
WRT the TMS320F280041C SDFM.. when running in mode=2, the TRM (last section of page 1690 (SPRUI33d ) states..
"When MOD=2, data and modulated clock signals are encoded into modulated data as shown in Mode 2 of Figure 17-4. In this mode, the clock input SD-Cx pin should be left floating. The input control unit performs continuous automatic calibration to achieve optimum decoding performance."
Customer asks.. "Must this (SD_Cx) pin physically be left floating or can I just use this pin for a different purpose?"
Thanks, Merril