I am trying to drive the motor via the MATLAB-Simulink platform.
Which GPIO pin should be used to enable/disable the inverter in the tmdxiddk379d board with F28379D Control Card?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am trying to drive the motor via the MATLAB-Simulink platform.
Which GPIO pin should be used to enable/disable the inverter in the tmdxiddk379d board with F28379D Control Card?
Pls review the user guide and schematics for such information.
Dear Ramesh,
Schematics of this board is bit confusing. Could you please tell me by looking at the attached images of schematics?
Regards,
Karthik
In the inverter macro M4, look for 'shutdown' signal and trace it backwards. You will see an OR gate taking signals from CC1 - GPIO-58. Suggest to spend some time to review the details.
Dear Ramesh,
Thanks a lot. It worked.
But there are two other signals connected to the OR gate (TripSafe, OCP-E). I guess OCP-E is used by Over Current Protection macro M6. I didn't understand why TripSafe is used to.
And also can we interface position encoder with 3 Hall sensors to TMDXIDDK379D?
HW guide says that only these position encoders are supported
1. QEP
2. Resolver
3. Sin-Cos
4. EnDat / BiSS
Regards,
Karthik
Since you opened another thread, am closing this thread. Btw, it is better to keep the topic to the query subject so that it helps someone in future to search and reach the answers to their queries.