Other Parts Discussed in Thread: RM57L843
Hi,
I want to use SPI communication between two TI controller RM57L8x(SPI master) and TMS320f280040(SPI slave).
I will get 3,16 byte data from master, so I configured CHARLEN as 16 and buffer length as 3 master mcu code.
I have configured TMS320f280040 as slave using below settings.
//GPIO config // SPISOMIA. // GPIO_setMasterCore(DEVICE_GPIO_PIN_SPISOMIA, GPIO_CORE_CPU1); GPIO_setPinConfig(DEVICE_GPIO_CFG_SPISOMIA); GPIO_setPadConfig(DEVICE_GPIO_PIN_SPISOMIA, GPIO_PIN_TYPE_PULLUP); GPIO_setQualificationMode(DEVICE_GPIO_PIN_SPISOMIA, GPIO_QUAL_ASYNC); // // SPISIMOA. // GPIO_setMasterCore(DEVICE_GPIO_PIN_SPISIMOA, GPIO_CORE_CPU1); GPIO_setPinConfig(DEVICE_GPIO_CFG_SPISIMOA); GPIO_setPadConfig(DEVICE_GPIO_PIN_SPISIMOA, GPIO_PIN_TYPE_PULLUP); GPIO_setQualificationMode(DEVICE_GPIO_PIN_SPISIMOA, GPIO_QUAL_ASYNC); // // SPISTEA. // GPIO_setMasterCore(DEVICE_GPIO_PIN_SPISTEA, GPIO_CORE_CPU1); GPIO_setPinConfig(DEVICE_GPIO_CFG_SPISTEA); GPIO_setPadConfig(DEVICE_GPIO_PIN_SPISTEA, GPIO_PIN_TYPE_PULLUP); GPIO_setQualificationMode(DEVICE_GPIO_PIN_SPISTEA, GPIO_QUAL_ASYNC); // // SPICLKA. // GPIO_setMasterCore(DEVICE_GPIO_PIN_SPICLKA, GPIO_CORE_CPU1); GPIO_setPinConfig(DEVICE_GPIO_CFG_SPICLKA); GPIO_setPadConfig(DEVICE_GPIO_PIN_SPICLKA, GPIO_PIN_TYPE_PULLUP); GPIO_setQualificationMode(DEVICE_GPIO_PIN_SPICLKA, GPIO_QUAL_ASYNC); //SPI configuration SPI_disableModule(SPIA_BASE); // // SPI configuration. Use a 500kHz SPICLK and 16-bit word size. // SPI_setConfig(SPIA_BASE, DEVICE_LSPCLK_FREQ, SPI_PROT_POL0PHA0,SPI_MODE_SLAVE, 500000, 16); // // FIFO and interrupt configuration // SPI_enableFIFO(SPIA_BASE); SPI_resetRxFIFO(SPIA_BASE); SPI_clearInterruptStatus(SPIA_BASE, SPI_INT_RXFF); SPI_setFIFOInterruptLevel(SPIA_BASE, SPI_FIFO_TX2, SPI_FIFO_RX3); SPI_enableInterrupt(SPIA_BASE, SPI_INT_RXFF); // // Configuration complete. Enable the module. // SPI_enableModule(SPIA_BASE);
// reception process
uiData = SPI_readDataBlockingFIFO(SPIA_BASE);
uiData is of type uint16_t
When I run the code and see in uiData in debug window, it is coming as 0.
I also verified the SPICLK,MOSI, CS signals on scope it is correct.
What I am missing while configuring slave mcu, am I am doing anything wrong configuration ?
Please help me in this.
Thanks
Pratik