Other Parts Discussed in Thread: C2000WARE
Hi Team,
My customer is evaluating F280049C Launchpad for one the applications and need to use peripherals like SPI-A, SPI-B, SCI-A, SCI-B etc along with some preprocessing and control loops. The execution periodicity is 10us which they are generating through CPUTimer0 interrupt. What is the easiest way to schedule different activities ? For eg, they need to use a GPIO to function as ChipSelect of SPI-A, another for SPI-B, 3rd one for SCI-A Transmit/Receive enable etc.
Not able to use the dedicated CS of these peripherals due to some other reasons. Customer want to enable SPI-A CS through GPIO at one point of time, start transmitting the data and disable the CS after transmitting data. They are not able to use delay functions in between since they need CPU cycles for other preprocessing functions.
Can you please help with your comments to address this issue.
Regards, Shinu.