This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSSOLARUINVKIT: TMDSSOLARUINVKIT: How to make it work.

Part Number: TMDSSOLARUINVKIT

Hi,

I have purchased this Solar Inverter Kit and am trying to make it work in Lab Environment. I have done the following steps so far:

1. Powered with 12 and 15V power supplies

2. Shorted TP8 and TP9

3. Connected a lab voltage supply (30V) between PV+ and PV-.

At this point, I was expecting to get a 110V output. But I am only able to measure ~100mVrms. What other steps do I need to follow. 

Also, I am not sure where to get the software to control the PCB, or which software to use as it did not come with any DVD or USB drives.