Hello,
I have connected three signals on ADCA
1. 5volt DC
2. 15volt DC
3. V_SENSE range(0-2V)
Out of above I am able to read 5V and 15V correctly.
However I am not able to read V_SENSE signal it is fluctuating(even if given input signal is constant i.e, 212mV).
V_SENSE connected to channel A10.
Configuration:
Interrupt setting:
ISR:
ADC channel read:
I am triggering ADC channel after every 10ms in main.
Please guide or add if I missed something in order to resolve the issue.