Hello,
is it possible to split the struct USER_Params from userParams.h into to 2 structs:
- one with all variables without errorCode as const, so that it is put into flash
- one that only contains the errorCode
I checked everything. The only one is the Estimator function CTRL_setEstParams, which uses the struct USER_Params. The function is in the estimator lib. Does this function write to the struct USER_Params or not. When not I can split it and give the function CTRL_setEstParams the pointer of the flash-struct.
Thanks for answering
regards
David