Dear team:
One of my customers has the following questions during the use of the kit:
1) In the program, the maximum voltage and current measurement ranges are respectively defined by macros as:
#define VAC_MAX_SENSE 620.152f
#define VDCBUS_MAX_SENSE 620.152f
#define I_MAX_SENSE 15.6f
2) The calculated values in the excel table are:
Vbus_max_sense = 451.65Volts
Vac_max_sense=450.15Volts
Imax_sense = 16.968Amps
May I ask why the software calculation and the hardware test are inconsistent?
Best regards