Hi
I meet a problem with F280023,
It works good when I load FW from XDS110, then when I reboot mcu, it got stuck ( XRSN generating low pulse continuous )
I checked something as below
1. GPIO24 and GPIO32, both of them are HI level
2.cmd file is 280023_FLASH_Lnk.cmd
3. VDDIO is 3.3V
4. The oscillator is INT_OSC2
what else should I need to check?
Thx