Other Parts Discussed in Thread: MOTORWARE
I have a similar case of this error here
I developed the project from Lab13 into a custom application that works on EVAL board LauchXL-F28069M with BOOSTXL-DRV8305 the code complies okay via XDS100 onboard. I then build the custom board, updated the FW to match the change of GPIO layout then updated the properties to match XDS200 external device. I note I had to update both boxes in the variants in order to get XDS200 connection list and it spew out error which I not familiar.
I have no clue how to resolve this error. The C2000 library is up to date.
error #16008-D: file
"E:/010_WorkAOT/011MyGit20/107_RVPPulser/Motorware/motorwareAOT_1_01_00_18/s
w/modules/fast/lib/32b/f28x/f2806x/2806xRevB_IQmath_BootROMSymbols.lib<TMS32
0x2806x_REVB_boot_rom_out___IQ24log_tmp.obj>" specifies ISA revision
"C2800", which is not compatible with ISA revision "C2700" specified in a
previous file or on the command line
error #16008-D: file
"E:/010_WorkAOT/011MyGit20/107_RVPPulser/Motorware/motorwareAOT_1_01_00_18/s
w/modules/fast/lib/32b/f28x/f2806x/2806xRevB_IQmath_BootROMSymbols.lib<TMS32
0x2806x_REVB_boot_rom_out___IQ24sinPU_tmp.obj>" specifies ISA revision
"C2800", which is not compatible with ISA revision "C2700" specified in a
previous file or on the command line
error #16008-D: file
"E:/010_WorkAOT/011MyGit20/107_RVPPulser/Motorware/motorwareAOT_1_01_00_18/s
w/modules/fast/lib/32b/f28x/f2806x/2806xRevB_IQmath_BootROMSymbols.lib<TMS32
0x2806x_REVB_boot_rom_out___IQ24sqrt_tmp.obj>" specifies ISA revision
"C2800", which is not compatible with ISA revision "C2700" specified in a
previous file or on the command line
error #16008-D: file
"E:/010_WorkAOT/011MyGit20/107_RVPPulser/Motorware/motorwareAOT_1_01_00_18/s
w/modules/fast/lib/32b/f28x/f2806x/2806xRevB_IQmath_BootROMSymbols.lib<TMS32
0x2806x_REVB_boot_rom_out___IQ24toF_tmp.obj>" specifies ISA revision
"C2800", which is not compatible with ISA revision "C2700" specified in a
previous file or on the command line