Other Parts Discussed in Thread: MOTORWARE
We recently purchased the above kit, it came with F2806xM isolated daugther card. I am going to power the kit with 110V AC using the 3-pin 85-132 VAC socket. Is the PFC-Booster block enabled by default? If I connect BS-1 -BS-3 and BS-4 -BS-5 as mentioned in the Hardware manual, would it supply 400 V DC to the invertor. I need to drive a 3 phase 230V ACIM.
Could not find any example code or GUI option.