Other Parts Discussed in Thread: C2000WARE
Hi all,
According to the TRM for the TMS320F28004x:
" If the DAC is used at any reference voltage other than 2.5v, the offset trim must be adjusted to ensure the offset error performance stays within the device-specific data manual limits. The DAC offset register is a 16-bit register that contains the 8-bit signed offset trim in the lower half of the register. Use the function call DAC_tuneOffsetTrim() found in C2000Ware to adjust the offset"
The only place where I can find this function is in the driverlib, and since we are not using driverlib in our project, is there another way two adjust the DAC offset?