This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-02002: PMP21553 & PMP21561 Versus TIDA-01605 Automotive Dual-Channel, SiC MOSFET Gate Driver With Two-Level Turnoff Protection

Part Number: TIDM-02002
Other Parts Discussed in Thread: TIDA-01605, PMP21553, PMP21561

I am working on the TIDM-02002 reference design and I came across TIDA-01605 (Automotive Dual-Channel SiC MOSFET Gate Driver With Two-Level Turnoff Protection).
I noticed the difference is that the primary and secondary side drivers (PMP21553 & PMP21561) have no short circuit detection & Two level Turn off protections. 

- I wonder how the SiC Mosfet Short circuit Detection is implemented in TIDM-02002,and does it meet the timing requirements?
- For the primary and secondary side gate drivers, is it better to use TIDA-01605 on the four legs?

Thanks in advance