Other Parts Discussed in Thread: POWERSUITE
Hi TI team,
We are testing Build 3 closed voltage & current loop demo mode with 110Vrms output voltage. In POWERSUITE setting, only changed Vout from default 220Vrms to 110Vrms, others are kept as default setting. The load for EVM is using an AC-to-DC PSU with PFC.
However, after increasing the DC input voltage from 0V to 380V slowly, then we found EVM having unstable output voltage when increasing PSU loading slowly from 0W to 240W. EVM will shut down with OverCurrent Trip if increasing from 240W to 264W, please refer to below waveforms for detail.
With PSU loading 240W, EVM has output voltage unstable
(CH1: Vds of Q2, CH2: Vds of Q4, CH3: Output voltage, CH4: Output current)
Modulation index=0.3871
Modulation index=0.5
With PSU loading 264W, EVM shut down with OverCurrent Trip
regards,
Cleto