This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

RTOS: Problem in procession of download . blind.out file

Tool/software: TI-RTOS

HI

I am studying  RTOS of c2000

I have installed RTOS of c2000 in ccs 6.2 .  then I read the student study PDF:

IN "TI _RTOS_Kernnel_Workshop_student"  , I read follow :

 

then ,I do lab1 with my f28069 card . but ,  I meet problem.  :  when I download  that " blink.out" of 28xx ,    it can not be end of download .

like this:

 out file.path:

 

ccs show :

 

My f28069 card is fine ,  i tested it  whith download other .out.file .

I do now why TI support that blink.out can no download , plese support me.

thanks

best regard !

hunk.

 

  • In reply to Ozino Odharo:

    Hi Hunk,

    Were you able to get this issue resolved?

    Regards,
    Ozino

  • In reply to Ozino Odharo:

    no. but I skiped it. thank you!
    there is an another question has not resolved in forum . please help me to push!
  • In reply to yanzhen fu:

    Hunk,

    Is this your other quesiton:
    " I want to know , Is RTOS 'S lab1 different with normal project without RTOS. ? or what will do the nest step I should do ?"

    If so, the answer would be that that lab 1's project is different from typical projects that use RTOS since the source code is not provided. In lab 1, the .out file is provided to only demonstrate how to load code to the board and to run code. This should not prevent you from continuing with the rest of the labs.

    If it is not your question, please ask it again. Thanks.

    Regards,
    Ozino

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.