This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TMDSRSLVR: Hardware Schematics Resolver interface

Intellectual 420 points

Replies: 5

Views: 482

Part Number: TMDSRSLVR

Hello TI,

I want to connect my Motor's Resolver to the TMDSRSLVR Eval. board. I have seen schematics and also attached below. I dont understand which one is which. How to connect sin +/- , cos +/- and excitation +/- to the J10 of the TMDSRSLVR board. 

Can anyone help me to clarify the interface?

Thank you.

regards

Rahul

  • Hi Rahul,

    Rahulkumar Lukhi
    I dont understand which one is which

    You mean pin mapping? If so here is the attached fig:

    Pins 1-2 : Sine

    Pins 3-4 : Cosine

    Pins 7-8 : Primary

    Regards,

    Gautam

     

    If a post answers your question, please click on "This resolved my issue" button

    Are You A Beginner or New to TI's C2000™ Family? Do Check This Book!

  • Hello,

    Looks like you are just starting. In general, swapping the winding +/- does not damage the board. For example, as long as you connect the sine winding terminals to pins 3 and 4 on J10, it is ok. A different combo of +/- will only alter the angle estimation and not damage the board. Remember, all the windings are electrically isolated within the resolver. Once you understand the setup, you can reconnect appropriately per your need.

  • In reply to Gautam Iyer:

    Hello Gautam,

    Thank you. I meant the pin mapping and I got it.

    regards
    Rahul
  • In reply to Stark:

    Perfect!

    Regards,
    Gautam

     

    If a post answers your question, please click on "This resolved my issue" button

    Are You A Beginner or New to TI's C2000™ Family? Do Check This Book!

  • In reply to Gautam Iyer:

    It's clearly seen but still Instead of Pins 7-8 : Primary , it is Pins 6-7: Primary.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.