This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TMDSRSLVR: SPI interface Jumper setting

Prodigy 45 points

Replies: 2

Views: 218

Part Number: TMDSRSLVR

Hello, 

I am using TMDSRSLVR kit with F28335 control card and I wanted to do SPI communication to other board. 

I set following modes on control card F28335.

SW1-OFF, SW2-ON.

Now the kit itself, I have connected my USB for code upload and power supply and SW1-ON. There is only one jumper which is placed and that is J9.

Also I have connected 1,3,5,7, 11 pin of J11 SPI interface of Resolver kit to another board's SPI which includes  STEN, SCLK, SIMO, SOMI and GND resp.

I am sending integer data from Kit to other TI board via SPI and fortunately I am not receiving any data from another SPI which I kept as a slave.

can anyone please confirm the jumper setting if there is missing one because I could not find any documentation which has information about all these setting.

-Jim

  • I don't see anything wrong with the jumper settings. If you are expecting a data from the slave SPI, the master has to provide the clock for it. You may have to revisit the algorithm.

  • In reply to Ramesh Ramamoorthy:

    Jim,

    Is the issue resolved? If so, pls close the post.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.