This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TMDSECATCNCD379D: Buying EtherCAT ET1100 board

Intellectual 455 points

Replies: 3

Views: 274

Part Number: TMDSECATCNCD379D

Dear TI Officer,

I am interested in the TMDSECATNCD379 EtherCAT Board. However, I only want to buy the EtherCAT board, because I have already got the TMS320F28379D control CARD. But there is only one option for me to buy both the EtherCAT board and the controlCARD ( 249$). Is it possible for me to buy the EtherCAT board only ? 

Regards,
An.

  • Unfortunately these are not sold separately.

  • In reply to ChrisClearman:

    Hello Chris,

    If it is so, can you recommend me some alternatives to the EtherCAT board ? Does any EtherCAT board can be connected to the TMS320F28379D board via the external connector J9 ( Hirose DF4HC(4.0)-60DS-0.4V(51)) ? 

    Regards,
    An.

  • In reply to Thuan Duong:

    An,
    J9 is a special connector defined only for the C2000 controlCARDS. I don't know of any other EtherCAT boards supporting this connector.

    Best Regards,

    Brian Fortman                  

    Industrial Drives and Automation              

    C2000 Microcontrollers

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.