This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TMS320F280049: DRV8312-69M-KIT with 280049 control card.

Expert 7650 points

Replies: 5

Views: 233

Part Number: TMS320F280049

Can DRV8312-69M-KIT be used with 280049 control card(TMDSCNCD280049C) for InstaSPIN evaluation?

If there are any limitation, please let me know.

 

Regards,

Furuya 

  • Kengo,

    Most of the TI engineers in C2000 team are on vacation. Please expect a reply after Jan 1 week.

    Regards,
    Manoj

    ---------------------------------------------------------------------------------------------------

    If a post answers your question, please mark it with the "verify answer" button.

    Other useful links:

    C2000 Getting Started      C2000 Flash Common Issues/FAQs      Emulation FAQ

     

  • In reply to Manoj Santha Mohan:

    Hi Furuya-san,

    The F280049C controlCARD should be able to physically plug into the DRV8312-69M-KIT, if the TMDSADAP180TO100 is used.  It appears that, if done, the F280049C MCU will have its peripherals in the right place that utilize the majority, if not all, of the features of the board.

    However, from a software perspective, there will not be any software that uses this configuration.  As such, you/customer would need to write software that would make the system work.  This may be a bit challenging.

    Note that InstaSPIN with the F28004x series is not currently supported:
    https://e2e.ti.com/support/microcontrollers/c2000/f/171/t/740747


    Thank you,
    Brett

  • In reply to Brett Larimore:

    Brett,

    Thank you for your answer.
    Customer plan to evaluate the below motor with DRV8312-69M-KIT.
    product.mabuchi-motor.co.jp/detail.html

    Could you let me know if DRV8312-69M-KIT has enough current and voltage capability to evaluate with it?

    Regards,
    Furuya
  • In reply to Kengo Furuya:

    Furuya-san,

             Instaspin is typically used with BLDC motors(Brush-less Direct Current motors).

    The link you sent was for a brushed motor(ブラシ付モータ) correct? Below is a link that talks about some of the potential draw backs of using a brushed motor with instaSPIN.

     

    C2000 can certainly drive a brushed motor without instaSPIN. However the kit referenced above was designed to work with BLDC motors.

    Regards,
    Cody 

    Getting Started with the C2000 ePWM module

  • In reply to Cody Watkins:

    Furuya-san,
    has this issue been resolved? Do you need further help?

    Regards,
    Cody

    Getting Started with the C2000 ePWM module

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.