This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

INSTASPINUNIVERSALGUI: Problem with initialization of InstaSPIN_MOTION_F2806xM

Prodigy 10 points

Replies: 1

Views: 56

Part Number: INSTASPINUNIVERSALGUI

Hello,

I have a problem with establishing comminucation with my LAUNCHXL-F28069M demoboard, trying to run it with BOOSTXL-DRV8301 motor driver board.

The FTDI chip on the LaunchXL board was reprogrammedby me, according to the recommendations from the doc  (http://www.ti.com/lit/ug/sprui11b/sprui11b.pdf  - Virtual COM port at channel B was enabled.  Now the PC (Windows 10) detects COM port with name "XDS100 Class USB Serial Port (COM11)". Also there are 2 devices in devicetree under heading: Texas Instr. Debug Probes, so the PC sees the debugger and COM-port.

The LaunchXL board loads successfully, and some demo-app prints out the temperature into the console, thus board and UART communication is OK.

I'm trying to load the InstaSPIN_MOTION_F2806xM.exe  application to start work with my DRV8301 and my bldc motors 2MTR-DYNO,  but on initialization I always see the same error - 

Restarting Program Model...
Initializing target : C:\ti\guicomposer\webapps\InstaSPIN_MOTION_F2806xM\appConfig.ccxml
Connecting target: Texas Instruments XDS100v2 USB Emulator_0/C28xx
sun.org.mozilla.javascript.internal.WrappedException: Wrapped com.ti.ccstudio.scripting.environment.ScriptingException: Error connecting to the target: emulation failure occurred (<Unknown source>#14) in <Unknown source> at line number 14Restart Completed.

So what can be wrong?  I do everything exclusively acc.to TI documentation, but with no results.

Regards,

Roman Fedoryak.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.