This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

CCS/TMS320F28379D: TMS320F28379D

Prodigy 100 points

Replies: 3

Views: 94

Part Number: TMS320F28379D

Tool/software: Code Composer Studio

Dear Sir 

Very Good Evening

I am working on grid connected single phase inverter code. After clicking on the buid option, it is showing the error: description Resource Path Location Type

devkits.HV_1PH_DCAC.Kit: no element named 'adcTriggerSource' .xdchelp /gridConnectedInverterLCLFltr line 21 C/C++ Problem. Give me some suggestion to solve this error.

  • Anup,

    What version of the solution are you using? Can you provide the version of powerSUITE you are using. Are you using the solution provided in the C2000Ware-DigitalPower-SDK?

    Regards,

    Ozino

  • In reply to Ozino Odharo:

    Dear Sir

    Very Good Morning

    I am using CCS Version -8 and the solution file is grid Connected inverter LCLFltr. This file is downloaded from Resource Explorer Classic. The application report is TIDUB21A Nov. 2015 - Revised Oct. 2016.

    PowerSUITE - 2_03_00_00

    Compiler version - 16.9.2.LTS

  • In reply to ANUP KUMAR:

    Anup,

    Thank you for the information. I will advise that you download the latest version of the C2000Ware-DigitalPower-SDK and use the version of the gridConnectedInverterLCLFltr example provided in there.

    Also update to the latest version of CCS and the c2000 compiler. Thanks.

    Regards,

    Ozino

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.