This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

CCS/TMDXIDDK379D: CCS Debug not working

Prodigy 40 points

Replies: 1

Views: 85

Part Number: TMDXIDDK379D

Tool/software: Code Composer Studio

I am new to this dev kit and I was following the user guide to try to understand it. However whenever I try to run the debugger, the enable flag resets to 0 in the expression window and nothing executes. This is what I see:

_______________________________________________________________________________________

_______________________________________________________________________________________

_______________________________________________________________________________________

_______________________________________________________________________________________

After looking online, This break might occur because the target is halted at "a program address where there is no source code correlation", or "the PC not being able to properly locate estimator functions in ROM", or "the CPU had executed illegal opcode."

But as i am new, i don't really understand how to fix the problem.

I tried to load the output file onto the device by going to Run->Load->Load Program but that also did not work when I actually ran the program.

What am i doing wrong?

user guide: http://www.ti.com/lit/ug/sprui44/sprui44.pdf

product: www.ti.com/.../TMDXIDDK379D

  • If you single step through the code once you get it loaded instead of just running it, can you determine the point at which this reset or illegal op code occurs?

    Thanks

    Whitney

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.