• Resolved

TMS320F2808: HOW TO BOOT FROM SCI

Prodigy 50 points

Replies: 8

Views: 148

Part Number: TMS320F2808

Hi,

I am using TMS320F2808, in the present configuration, we are made GPIO18, GPIO29, and GPIO34 HIGH so it will boot from FLASH it is working fine. The code which I was flashed into the device is running from the flash. Now we are trying to use the SCI boot option so will make GPIO pin status GPIO18, GPIO29 HIGH, and GPIO34 LOW.

  • My question is how to program my .out file into the device flash in SCI boot mode.
  • what is the tool used for flashing .out, In the SCI boot mode?
  • Is there any changes required in the current program.
  • Please provide any documentation is available for booting from SCI.

Thanks in advance, waiting for replay.

With regards,

Sivakrishna