This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28030 ADC Clock

What is the maximum ADC clock for F28030 with 500nS ADC Conversion time?

Is it 26MHz? 

  • Hi Suttichai-

    The maximum ADC clock is 60Mhz, but the minimum ACQPS for 28030 is 23 ( 24 ADC clock cycles ).  ADC conversion time is 13 cycles, seven of which overlap with the S/H in normal OVERLAP mode.  That leaves six cycles which are not overlapped, so the minimum sample/conversion time for 28030 is 24+6=30 cycles.  At 60Mhz this is 500ns.

     

    best regards,

    Joe