This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem programming OTP piccolo TMS320F2806x

Other Parts Discussed in Thread: TMS320F28021, CONTROLSUITE

Hi,
I am using XDS100v2, under CCSv4, and when I want to program my boot variables in order to boot from SPI I have the following message:
 C28xx: Flash Programmer: Error encountered when writing to flash memory
C28xx: Trouble Writing Memory Block at 0x3d7bfc on Page 0 of Length 0x2 
Cannot write to target

My configurations are the following:
I have defined two constants at 0x3D7BFB and 3D7BFE, such as:

#pragma DATA_SECTION(BootModeValue, "BootMode");
const long BootModeValue = 0x0004;

#pragma DATA_SECTION(KeyBootValue, "KeyBoot");
const long KeyBootValue = 0x005A;

OTP         : origin = 0x3D7800, length = 0x0003FB     /* on-chip OTP */

KEY_BOOT : origin = 0x3D7BFB, length = 0x000003 /* Key Boot value in OTP */
BOOT_MODE : origin = 0x3D7BFE, length = 0x000003 /* Boot mode selection */

BootMode : > BOOT_MODE, PAGE = 0
KeyBoot : > KEY_BOOT, PAGE = 0
When I look at my memory, I can see that BOOT_MODE value has well be set, but not my KEY_BOOT(0xFFFF)... Which leads to error message.
My device was never used before I programmed it one time, and had this error code.
So, can you explain me why I can't program my OTP, or the way to do it?

Thank you,

Éric