Other Parts Discussed in Thread: REF3225, TMS320F28035
Hi all,
I am working on the F28035 Piccolo controlcard and evaluating the ADC.
To avoid the influence of layout, GND and so on, I was running "Example_2803xAdcTempSensor" (I think we won't get better and shorter ADC connection than the internal temperature sensor) and got results varying in the range of 15 digits.
This is 15/4096 = 0,36% !!
I think this is too much - especially when regarding the fact that ADC accuracy should be a decade higher than the final result - this would give me an accuracy of the final result of no more than 3.6%, not regarding static errors.
I have really bad experience with the F2812 ADC and thought the 280x ADCs should be better...
So my question is: Are these 15 digits noise what I can expect? Can I reduce the noise somehow? Has somebody else experience with the Piccolo ADC accuracy and noise?