Other Parts Discussed in Thread: TMS320F2808, CCSTUDIO, SPRC191
Hello,
i'm new in Texas instrument applications and i'n following the tutorial. I'm working with MS320C200DSC Experimenter Kit: docking station and plug-in controlCARD with TMS320F2808. I use USB2000 CONTROLLER Blackhawk and developing with CCStudio versione 3.3.82.13.
Everyting seems to work (properly selected from Setup CCStudio and kit connected ), but when i have to load the targhet on cip te following message appears:
"Data verification failed at address 0x3FFFC0.
please verify targhet memory and memory map".
my .cmd file is:
MEMORY
{
PAGE 0 : PROG(R) : origin = 0x3E8000, length = 0x10000
PAGE 0 : BOOT(R) : origin = 0x3FF000, length = 0xFC0
PAGE 0 : RESET(R) : origin = 0x3FFFC0, length = 0x2
PAGE 0 : VECTORS(R) : origin = 0x3FFFC2, length = 0x3E
PAGE 1 : M0RAM(RW) : origin = 0x000000, length = 0x400
PAGE 1 : M1RAM(RW) : origin = 0x000400, length = 0x400
PAGE 1 : L0L1RAM(RW) : origin = 0x008000, length = 0x2000
PAGE 1 : H0RAM(RW) : origin = 0x3F8000, length = 0x2000
}
SECTIONS
{
/* 22-bit program sections */
.reset : > RESET, PAGE = 0
.vectors : > VECTORS, PAGE = 0
.pinit : > PROG, PAGE = 0
.cinit : > PROG, PAGE = 0
.text : > PROG, PAGE = 0
/* 16-Bit data sections */
.const : > L0L1RAM, PAGE = 1
.bss : > L0L1RAM, PAGE = 1
.stack : > M1RAM, PAGE = 1
.sysmem : > M0RAM, PAGE = 1
.cio : > M0RAM, PAGE = 1
/* 32-bit data sections */
.ebss : > H0RAM, PAGE = 1
.econst : > H0RAM, PAGE = 1
.esysmem : > H0RAM, PAGE = 1
}
This file seems to me define correcty the memory map of TMS320F2808.
Any suggestion? Thank everyone.
Massimiliano