I have boththe "DRV8312 Motor Control Kit" and "F28069 Piccolo Experimenter Kit". Now I would like put the F28069 controlCARD from the experimenter kit into the DRV8312 board. When I try to use an XDS510LC USB JTAG device, I'm not able to create the target configuration.
Is this a supported configuration (DRV8312 board, F28069 controlCARD, XDS510LC)?
Is there a better/different JTAG emulator?