Other Parts Discussed in Thread: UNIFLASH
If you have received Rev A/Rev B samples of Concerto devices, the attached XML files will need to be placed in the following Code Composer directory in order to enable programming: These XML files will also work with Rev 0 silicon.
<CCS install directory>\ccs_base\c2000\nowFlash\configs.
If you are using UniFlash, the updated xmls should go to: uniflashv2\ccs_base\c2000\nowFlash\configs.
Alternatively, you can install device support updates from CCS5 help menu (check for updates) and these latest xmls will be placed at ccsv5\ccs_base\c2000\nowFlash\configs. But for UniFlash, these xml files have to be manually placed at above mentioned Uniflash path for now. We will work to update the UniFlash installer to include the latest xml files.
edit: The above files are for CCS V5.